This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can CCS 3.3 use SYS/BIOS?

Anonymous
Anonymous


Hi All,

I have found CCS 4 sometimes turns to be extremely slow on my old XP desktop computer, so I would like to switch back to CCS 3.3.

Does CCS 3.3 support higher versions of SYS/BIOS? It seems that SYS/BIOS (the v6.x version, not just DSP/BIOS) is created as a product of RTSC and is configured by XDCTools, both are closely related with eclipse. If I intend to roll back to CCS 3.3 which is not based on eclipse, can I still use it?



Sincerely,
Zheng

  • BIOS 6.x should be used with CCSv4.

    How much memory does your computer have?   We recommend that you update to at least 2MB.   XP will support up to 3MB so I would recommend going for 3MB (you might have to buy 4MB and 1MB will be unused).  Memory is relatively inexpensive and will make a huge difference.

    If build time is the problem, then 2 suggestions:

    (1)  use debug profile for building until you need to optimize for performance.   Debug builds are much faster than whole_program builds.

    (2)  make sure that you use the "build" option (not "rebuild"!).  rebuild will clean the project and then rebuild the whole project -- including the BIOS configuration and partial link.  "build" is smarter and will only build the files that have changed or have dependency on a file that has changed.

    Regards,
    -Karl-

  • Anonymous
    0 Anonymous in reply to Karl Wechsler

    Dear Karl,

    I have found that sometimes the problem is due to the existence of a large array in the "watch" window. For example, if I add an array of 10000 elements into the watch window, even if this array is not expanded, CCS 4 would still be very slow. Removing the array from "watch" improves the speed.

     

    Zheng