This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMIC120: AMIC120 motor control with real time monitoring

Genius 5840 points

Hello,

I'd like to monitor positions and speed graphically in real time while working on the motor_control example of the industrial drive package.
Is there a good solution to do the above?

Regards,

U-SK

  • Unfortunately we do not currently have a method to show the values graphically. We are investigating internally if the graphing capability of CCS can be used but so far the need for a breakpoint to update the graph is affecting the real-time performance of the control loop.

    I'll respond here if we find a better solution.

    Thanks for the feedback and it is definitely something that we are looking to provide in future examples.

    Jason Reeder