This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

minimum time for release of reset after powerup on OMAPL-138

Other Parts Discussed in Thread: TPS65070, OMAP-L132

I would like to minimise the boot time when using the OMAPL-138

I can find nothing in the documentation regarding when RESET can be de-asserted after power up - other than the voltages must have stabilized and the reset must be low for a minimum of 100ns.

The PMIC used on the LogicPD EVM uses the TPS65070 which releases reset only 400ms after the last supply has stabilized. Are there any other considerations than stable power - clock  maybe -  that would require a 0.4 sec delay?

Thanks

Steve