Part Number: AM3352
Tool/software: Linux
Hello.
On the AM335x custom board like GPEVM. Linux is ti-processor-sdk-linux-rt-am335x-evm-04.03.00.05.
I want to work external RTC(RICOH,R2023). So I customize kernel configs:
1. in menuconfig : Device Drivers --> Real Time Clock --> <*> Ricoh R2025S/D, RS5C372A/B, RV5C386, RV5C387A
(Because R2023 is seemed to be like R2025.)
2. in devicetree entry, R2023 is connected to i2c0 bus line so I wrote DT entry like below:
&i2c0 {
pinctrl-names = "default";
pinctrl-0 = <&i2c0_pins>;
status = "okay";
clock-frequency = <400000>;
r2023: r2023@32 {
status = "okey";
compatible = "ricoh,rs5c372";
reg = <0x32>;
};
};
I checked i2c0 works fine, and I can read 0x32 slave address by using i2cdump command.
When I look at the dmesg log, the device r2023 seems to be probed. (Only omap-rtc is probed.)
Any mistake is there?
I want your advice to resolve this probrem.
dmesg log is share-log-1119.zip
Regards.
Nishihashi