This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

In C5510 DSK, can I use memory expansion connector to connect ADC directly???

        I want to use C5510 DSK to read data from ADC7813, whcih has 9 output pin(8 data pins and 1 busy signal pin)  and 3 control pins.

       Since the HPI Expansion Connector has only 3 GPIO pins, can I use the data bus D[31:0] in "Memory Expansion Connector", or HD[15:0] in HPI Expansion Connector,  connecting the ADC pins???

        If yes, how can I read data from or write control signal to D[31:0] or HD[15:0]???

       By the way, which  connector can connect  "Memory Expansion Connector"(80 pins) and ADC7813????