Hi Team,
Does sitara support TSN and OPC UA on the same time? If not, do we have this plan?
I know AM5728 support OPC UA and AM65xx support TSN. But I can't see a chip can support both. Do you have any suggestions?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Does sitara support TSN and OPC UA on the same time? If not, do we have this plan?
I know AM5728 support OPC UA and AM65xx support TSN. But I can't see a chip can support both. Do you have any suggestions?
Thanks!
Hi Eggsy, AM65xx should be able to support both. Matricon OPC UA SDK can be configured/scaled down to have a small memory footprint (could even run in an MCU). About Eth interfaces cababilities AM65xx offers Gb Eth port and up to 6 PRU-ICSS Gb ports
Thank you,
Paula
Hi Paula,
Thanks for your feedback. And I have some below questions from customers.
Thanks for your help!
Hi Eggsy, please see my comments below
PC-- No
PC-- Potentially yes, as Matrikon OPC is scalable. However, currently it is only supported/tested on AM572x with Linux. For other devices and OSes the customer would need to contact Matrikon
PC-- Yes
PC-- No, it is commercial. One Open Source alternative is OPC62441 stack
PC-- Yes this is in the roadmap. I will try to find out schedule and come back to you.
PC-- Yes, this is the roadmap
thank you,
Paula