Other Parts Discussed in Thread: TPS65950
Hello,
i want to use the A11-A13, A15 pins on the Expansion Connector P7 for frequency-measurement. The EVM manual tells me (page 25), that i have to set T2_GPIO_2 high and GPIO_61 also high, so i get these signals on the expansion connector (because these pins are multiplexed with USB-functions, which i don't need). GPIO_61 is no problem, but T2_GPIO_2 is controlled via the TPS65950, which is connected via I2C to the OMAP.
Do i really have to work on a I2C-solution for communication with the power module, or is there already some kind of tool i can use?