Hi,
May I know the csi cameras supported on tda3xevm to run single camera usecases?
Regards,
Anil
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
May I know the csi cameras supported on tda3xevm to run single camera usecases?
Regards,
Anil
VisionSDK_UserGuide_TDA3xx.pdfHi Anuj,
Thanks for the reply.
I had gone through the vision sdk userguide,it mentioned as ov10635 parallel sensor be used for vip based usecases.
Please find the attached userguide (section 2.5).
Regards,
Anil
Hi,
Yes, you are right.
on the usecase menu under single camera usecase, you call run all usecase of vip capture except the ones which mentioned as HDMI.
After boot up press 1 and you will see below options
[IPU1-0] Single Camera Usecases
[IPU1-0] ------------------------
[IPU1-0] 1: 1CH VIP capture + Display
[IPU1-0] 2: 1CH VIP capture + Alg Frame Copy (DSP1) + Display
[IPU1-0] 3: 1CH VIP capture + Alg Frame Copy (EVE1) + Display
[IPU1-0] 4: 1CH VIP capture + Alg Frame Copy (A15) + Display
[IPU1-0] 5: 1CH VIP capture + Edge Detect (EVE1) + Display
[IPU1-0] 6: 1CH VIP capture + Dense Optical Flow (EVEx) + Display (HDMI)
[IPU1-0] 7: 1CH VIP capture (HDMI) + Sparse Optical Flow (EVE1) + Display
[IPU1-0] 8: 1CH VIP capture + Alg Subframe Copy (EVE1) + Display
[IPU1-0] 9: 1CH VIP capture + DSSWB + CRC + Display (Supported only on TDA3x)
[IPU1-0] b: 1CH VIP capture (HDMI) + Lane Detect (DSP1 + EVE1) + Display
[IPU1-0] c: 1CH VIP capture (HDMI) + SOF (EVE1) + SFM (DSP1) + Display
[IPU1-0] d: 1CH VIP capture (HDMI) + Traffic Light Recognition (TLR) (DSP1) + Display
[IPU1-0] e: 1CH VIP capture (HDMI) + Pedestrian, Traffic Sign, Vehicle Detect 2 (EVE1 + DSP1) + Display
[IPU1-0] f: 1CH VIP capture (HDMI) + FrontCam Analytics 2 (PD+TSR+VD+LD+TLR+SFM) (DSPx, EVEx) + Display (HDMI)
[IPU1-0] g: 1CH VIP capture + QM Alg Frame Copy with FFI (DSP1) + Display
[IPU1-0] h: 1CH VIP capture + QM Alg Frame Copy with FFI (EVE1) + Display (TDA3x only)
[IPU1-0] i: 1CH VIP capture + Safe Frame Copy (A15) + Display
[IPU1-0] l: 1CH VIP capture + DisplayMultiPipe + DSSWb + Metadata
and you can use almost all usecase except 7,b,c,d,e,f.
Regards,
Anuj