Hi,
We have a custom board TCI6614, Ethernet running on Port0. NIMU and Platform library are rebuilt in accordance with the custom board, the example helloWorld from the NDK package works fine, but the emacExample (pdk_tci6614_1_02_01_03\packages\ti\drv\pa\example\emacExample\) does not work, falls into the function Add_MACAddress() in the pa_mgmt.c file with the error "Time to wait for a response from PA to the Pa_addMac command".
e2e.ti.com/.../421701 did not help.
I reset the power every time I load a project to the board, the SERDES and others init in accordance with the custom .gel file.
Thanks