This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Questions about OMAPL137,can ARM do signal processing and logic control at the same time

Hi there,

  I wonder If the ARM core is powerful enough to do the signal processing that DSP does.Cause the ARM core's frequecy is 300MHZ,If I just run some simple control task,Can ARM do the digital signal processing part,meaning that It can do fft or some complicated algorithm while running a system.If so,we can remove the DSP or just ignore him.I'm using OMAPL137 do USB data transfer ,think that a system running on ARM side can simplify the job rather than the DSP side?

  As far as I know,there are not so many people using OMAP processors,also the Davicci architecture.Could you please give the some details of the outstanding perspects of the two-core architecture of OMAP series?

 

Best regards

Calm