Other Parts Discussed in Thread: AM5728,
Champs,
Customer moved from AM5728 to AM5748 on exact same board and runs exact same (RTOS based ) binary that ran on AM5728. With AM5748 they observe power consumption going over 2W higher than AM5728 (1.36 vs 3.6W)! To understand the reason we ran PET on their use case for both devices and PET simulation confirmed the measurements. The use case is fairly simple ( single A15 core, DSS, QSPI/SPI/UARTs). Questions I have are
1. it looks like AM5748 PET does not permit running single A15 and shutting down the second one. Is it not possible in the AM5748 silicon?
2. AM5748 PET does not permit disabling C66s but puts them into AutoCG mode - what exactly does it mean? Do C66x consume considerable power in this state? is it possible to shut them down completely?
3. Can powered-up second A15 not running any firmware and C66x in AutoCG state account for >2W extra consumption?
The extra 2W causes serious unanticipated thermal issues in customer's system, so any insights will be greatly appreciated!
thanks
Michael