Part Number: AM3357
Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI-RTOS
Hello,
I am trying to add the full Ethernet/IP stack from Molex into the PRU ICSS Ethernet/IP example app. The example comes with a lib (libethernetip_adapter_stack_AM335x_arm.a).
There is some doc on how to replace the EIP example with the Molex delivery stack? I'm facing some issues with that. I suppose there are OS specific files, an adaptation layer, which are inside the lib that are missing or I'm not able to find. Which modifications were done by TI? Where can I find those files now that I have the license?
Furthermore, the current Molex stack version that I have is the 3.5.0, which is newer than the one which is in the example app (3.3.3).
Is the 3.5.0 version supported? Does it need some different adaptation layer?
Best regards,
Jordi