This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/AM5728: Boot up issue and matrix GUI support

Part Number: AM5728

Tool/software: TI-RTOS

Hi

Can someone please help me to solve this boot up issue.I am using AM5728 EVM and RTOS process SDK 5_00_00_15.

I have followed instructions in this link to boot from SD

linux SD Card Creation Guide in .

following are the messages observed in the serial port terminal
please help me to solve this issue

**** PDK SBL **** SBL Revision: 01.00.09.01 (Jul 27 2018 - 02:55:26) Begin parsing user application SD Boot - file open completed successfully Jumping to user application... SetPhyMode:000021e1 Auto:1, FD10:64, HD10:32, FD100:256, HD100:128, FD1000:8192 LPBK:0 Enter Ipc_start SetPhyMode:000021e1 Auto:1, FD10:64, HD10:32, FD100:256, HD100:128, FD1000:8192 LPBK:0 Ipc_start OK Ipc_attach() OK ipc_heap_init OK Image Processing Demo is Ready, EVM IP Addr ENETPHY_FindingState: PhyNum: 1 ENETPHY_FindingState: PhyNum: 2 ENETPHY_DisablePhy(1) Enable Phy to negotiate external connection NWAY Advertising: FullDuplex-1000 FullDuplex-100 HalfDuplex-100 FullDuplex-10 HalfDuplex-10 ENETPHY_DisablePhy(2) Enable Phy to negotiate external connection NWAY Advertising: FullDuplex-1000 FullDuplex-100 HalfDuplex-100 FullDuplex-10 HalfDuplex-10 Negotiated connection: FullDuplex 1000 Mbs Network Added: If-1:192.168.1.231

2) Do we have Matrix GUI and QT support in RTOS SDK?

Thanks,
Jahnavi