This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm6467 video applications



Good morning,

We are evaluating a dm6467 EVM for graphical applications and HD video processing.

The EVM comes with an X server for a frame buffer device (/dev/fb/...), which it cannot find. The davinci kernel drivers only seem to support fbdev on dm355 and dm644x. What is the supported route for running an X server and various graphical applications on the 6467?

Thanks,

Olivier

  • Oliver,

    The video display driver on DM6467 is based on V4L2 (as opposed to frame buffer as in DM644x) Linux standard.  I am not sure if X Server can run on top of V4L2; otherwise, you may need to port a frame-buffer driver to DM6467.  Please note that from a hardware perspective, display hardware on DM6467 is very different that what is found in DM6446 (build-in OSD hardware).