Our product uses a C5416 and we use HPI boot mode to load the code from our host. The INT2 flag is tied active so it is forced to HPI Boot. In this mode, we know the host can write to the DSP memory, but can the host do valid memory read accesses in this mode as well after the DSP is taken out of reset?