Other Parts Discussed in Thread: CCSTUDIO
hi all
i am studying the xdais standard.the software is ccs v3.3,and the configtion is C6412 Device Cycle Accurate Simulator.i think that the project in the codec_engine_1_10_01 is accord with the xdais standard.
so i build a videnc1.pjt.the file in the project is videnc1_copy.c、videnc1_copy_ti.h、videnc1_copy_ti_priv.h and affiliated head files,and the videnc1.tcf is copied from the figtest.tcf(the version is xdais_4.0d).but when rebuild all,there is errors.the compiling result is:
---------------------------- videnc1.pjt - Debug ----------------------------
[videnc1.tcf] "C:\CCStudio_v3.3\bios_5_31_02\xdctools\tconf" -b -Dconfig.importPath="C:/CCStudio_v3.3/bios_5_31_02/packages" videnc1.tcf
[videnc1_copy.c] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -g -q -fr"C:/xdm/videnc1/Debug" -@"Debug.lkf" "videnc1_copy.c"
"videnc1_copy.c", line 51: warning: a value of type "XDAS_Int32 (*)(IVIDENC1_Handle, XDM_BufDesc *, XDM_BufDesc *, IVIDENC1_InArgs *, IVIDENC1_OutArgs *)" cannot be used to initialize an entity of type "XDAS_Int32 (*)(IVIDENC1_Handle, IVIDEO1_BufDescIn *, XDM_BufDesc *, IVIDENC1_InArgs *, IVIDENC1_OutArgs *)"
[videnc1cfg.s62] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -g -q -fr"C:/xdm/videnc1/Debug" -@"Debug.lkf" "videnc1cfg.s62"
[videnc1cfg_c.c] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -g -q -fr"C:/xdm/videnc1/Debug" -@"Debug.lkf" "videnc1cfg_c.c"
[Linking...] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -@"Debug.lkf"
<Linking>
undefined first referenced
symbol in file
--------- ----------------
_main C:/CCStudio_v3.3/bios_5_31_02/packages/ti/bios/lib/bios.a64
>> error: symbol referencing errors - './Debug/hellodsp.out' not built
>> Compilation failure
Build Complete,
2 Errors, 1 Warnings, 0 Remarks.
how i do with it?