Part Number: PROCESSOR-SDK-AM335X
Tool/software: Linux
We've a custom board based on AM335x-EVM-SK. We are using ti-processor-sdk-linux-am335x-evm-05.00.00.15.
We tested the following 3 interfaces to prove its working to our customer. They're specifically asking about EDMA interface test along with its throughput.
1. I2C tested with external IC.
#include <stdio.h>
#include <stdint.h>
#include <unistd.h>
#include <stdlib.h>
#include <getopt.h>
#include <string.h>
#include <fcntl.h>
#include <sys/ioctl.h>
#include <linux/types.h>
#include <linux/spi/spidev.h>
static uint8_t mode;
static uint8_t bits = 8;
static uint32_t speed = 500000;
static uint16_t delay;
const char *device = "/dev/spidev0.0";
#define ARRAY_SIZE(a) (sizeof(a) / sizeof((a)[0]))
char buf[10];
char buf2[10];
int com_serial;
int failcount;
struct spi_ioc_transfer xfer[2];
struct spi_ioc_transfer xfer1[2];
void spi_write(int file)
{
unsigned char buf[32];
int status;
memset(buf, 0, sizeof buf);
buf[0] = 0x06;
xfer1[0].tx_buf = (unsigned long)buf;
xfer1[0].len = 1; /* Length of command to write*/
status = ioctl(file, SPI_IOC_MESSAGE(1), xfer1);
if (status < 0)
{
perror("SPI_IOC_MESSAGE");
return;
}
buf[0] = 0x01;
buf[1] = 0x30;
xfer1[0].tx_buf = (unsigned long)buf;
xfer1[0].len = 2; /* Length of command to write*/
status = ioctl(file, SPI_IOC_MESSAGE(1), xfer1);
if (status < 0)
{
perror("SPI_IOC_MESSAGE");
return;
}
printf("env: %02x %02x\n", buf[0], buf[1]);
// printf("ret: %02x %02x %02x %02x\n", buf2[0], buf2[1], buf2[2], buf2[3]);
com_serial=1;
failcount=0;
}
char * spi_read(int file)
{
int status;
memset(buf, 0, sizeof buf);
memset(buf2, 0, sizeof buf2);
buf[0] = 0x05;//0x9E;
// buf[1] = 0x00;
// buf[2] = 0x00;
// buf[3] = 0x00;
xfer[0].tx_buf = (unsigned long)buf;
xfer[0].len = 1; /* Length of command to write*/
xfer[1].rx_buf = (unsigned long) buf2;
xfer[1].len = 1; /* Length of Data to read */
status = ioctl(file, SPI_IOC_MESSAGE(2), xfer);
if (status < 0)
{
perror("SPI_IOC_MESSAGE");
return 0;
}
//printf("env: %02x %02x %02x\n", buf[0], buf[1], buf[2]);
printf("ret: %02x\n", buf2[0]);
}
int main(int argc, char *argv[])
{
int file;
if ((file = open(device,O_RDWR)) < 0)
{
printf("Failed to open the bus.");
/* ERROR HANDLING; you can check errno to see what went wrong */
exit(1);
}
printf("success to open the bus.");
if (ioctl(file, SPI_IOC_RD_MODE, &mode) < 0)
{
perror("SPI rd_mode");
return 0;
}
// if (ioctl(file, SPI_IOC_RD_LSB_FIRST, &lsb) < 0)
// {
// perror("SPI rd_lsb_fist");
// return;
// }
if (ioctl(file, SPI_IOC_WR_BITS_PER_WORD, &bits)<0)
{
perror("can't set bits per word");
return 0;
}
if (ioctl(file, SPI_IOC_RD_BITS_PER_WORD, &bits) < 0)
{
perror("SPI bits_per_word");
return 0;
}
if (ioctl(file, SPI_IOC_WR_MAX_SPEED_HZ, &speed)<0)
{
perror("can't set max speed hz");
return 0;
}
if (ioctl(file, SPI_IOC_RD_MAX_SPEED_HZ, &speed) < 0)
{
perror("SPI max_speed_hz");
return 0;
}
printf("spi mode %d, %d bits, %d Hz max\n",mode, bits, speed);
// transfer(file);
spi_write(file);
// spi_read(file);
return 0;
}
2. SPI tested with external NOR Flash. In this code, we're reading and writing at different times. not simultaneously.
#include <stdio.h>
#include <stdint.h>
#include <unistd.h>
#include <stdlib.h>
#include <getopt.h>
#include <string.h>
#include <fcntl.h>
#include <sys/ioctl.h>
#include <linux/types.h>
#include <linux/spi/spidev.h>
static uint8_t mode;
static uint8_t bits = 8;
static uint32_t speed = 500000;
static uint16_t delay;
const char *device = "/dev/spidev0.0";
#define ARRAY_SIZE(a) (sizeof(a) / sizeof((a)[0]))
char buf[10];
char buf2[10];
int com_serial;
int failcount;
struct spi_ioc_transfer xfer[2];
struct spi_ioc_transfer xfer1[2];
void spi_write(int file)
{
unsigned char buf[32];
int status;
memset(buf, 0, sizeof buf);
buf[0] = 0x06;
xfer1[0].tx_buf = (unsigned long)buf;
xfer1[0].len = 1; /* Length of command to write*/
status = ioctl(file, SPI_IOC_MESSAGE(1), xfer1);
if (status < 0)
{
perror("SPI_IOC_MESSAGE");
return;
}
buf[0] = 0x01;
buf[1] = 0x30;
xfer1[0].tx_buf = (unsigned long)buf;
xfer1[0].len = 2; /* Length of command to write*/
status = ioctl(file, SPI_IOC_MESSAGE(1), xfer1);
if (status < 0)
{
perror("SPI_IOC_MESSAGE");
return;
}
printf("env: %02x %02x\n", buf[0], buf[1]);
// printf("ret: %02x %02x %02x %02x\n", buf2[0], buf2[1], buf2[2], buf2[3]);
com_serial=1;
failcount=0;
}
char * spi_read(int file)
{
int status;
memset(buf, 0, sizeof buf);
memset(buf2, 0, sizeof buf2);
buf[0] = 0x05;//0x9E;
// buf[1] = 0x00;
// buf[2] = 0x00;
// buf[3] = 0x00;
xfer[0].tx_buf = (unsigned long)buf;
xfer[0].len = 1; /* Length of command to write*/
xfer[1].rx_buf = (unsigned long) buf2;
xfer[1].len = 1; /* Length of Data to read */
status = ioctl(file, SPI_IOC_MESSAGE(2), xfer);
if (status < 0)
{
perror("SPI_IOC_MESSAGE");
return 0;
}
//printf("env: %02x %02x %02x\n", buf[0], buf[1], buf[2]);
printf("ret: %02x\n", buf2[0]);
}
int main(int argc, char *argv[])
{
int file;
if ((file = open(device,O_RDWR)) < 0)
{
printf("Failed to open the bus.");
/* ERROR HANDLING; you can check errno to see what went wrong */
exit(1);
}
printf("success to open the bus.");
if (ioctl(file, SPI_IOC_RD_MODE, &mode) < 0)
{
perror("SPI rd_mode");
return 0;
}
// if (ioctl(file, SPI_IOC_RD_LSB_FIRST, &lsb) < 0)
// {
// perror("SPI rd_lsb_fist");
// return;
// }
if (ioctl(file, SPI_IOC_WR_BITS_PER_WORD, &bits)<0)
{
perror("can't set bits per word");
return 0;
}
if (ioctl(file, SPI_IOC_RD_BITS_PER_WORD, &bits) < 0)
{
perror("SPI bits_per_word");
return 0;
}
if (ioctl(file, SPI_IOC_WR_MAX_SPEED_HZ, &speed)<0)
{
perror("can't set max speed hz");
return 0;
}
if (ioctl(file, SPI_IOC_RD_MAX_SPEED_HZ, &speed) < 0)
{
perror("SPI max_speed_hz");
return 0;
}
printf("spi mode %d, %d bits, %d Hz max\n",mode, bits, speed);
// transfer(file);
spi_write(file);
// spi_read(file);
return 0;
}
3. EDMA tested with sample application(dmatest) provided in the sdk using modprobe dmatest timeout=200 iterations=500 run=1 verbose=on.
One thing i want to know is that is this transferring data within processor's memory or between processor and FPGA?
Now, we want to test all these 3 interfaces with FPGA i.e. to send and receive data to and from FPGA.
Please suggest me changes in my codes.
Any help in this regard is appreciated as we're in a strict time restriction.
Thank You.