Part Number: TMS320C6748
Other Parts Discussed in Thread: OMAP-L138,
Hello,
I need to sample an RF signal at 20 Mhz, and am wondering if a TMS320C6748 (via OMAP-L138) is going to adequate by itself, or whether external logic is required via FPGA, etc. What would be the options for sampling at this speed ... could the McASP be connected to an ADC, to get 16 bit resolution at 20 Mhz? (from what I have seen so far, maybe not). If not that, then is the uPP the only other option? And there, I haven't see an option for 16 bit at that speed (lower 12, maybe 14 bit resolution).
Also, could the samples be streamed to the DDR2 memory in real-time, for processing?
Please advise,
Robert