This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TMS320C5535: About HWI Object Property "Interrupt Mask" Settings of C5000 Connected Audio Framework

Part Number: TMS320C5535

Tool/software: TI-RTOS

Hi Champs,

According to a description of C55x DSP/BIOS 5.x API RG(SPRU404Q) below, when using "self" I have to set both interruptMask0 and interruptMask1 to "self".

   o C55x DSP/BIOS 5.x API RG [SPRU404Q AUG12]
    (www.ti.com/lit/ug/spru404q/spru404q.pdf)

     - Page 158

       ・ Interrupt Mask.


          ...When using "self", set both interruptMask0 and interruptMask1 (and iMirMask if the platform is OMAP 2320/2420) to "self".

However, in C5000 Connected Audio Framework, the HWI_INT20(USB) settings are below.
Are these the wrong settings? Do I have to fix it?



Regards,
J-breeze