Tool/software: TI-RTOS
Hello ,
I am using PROCESSOR_SDK_VISION_03_00_00_00 sdk and want to know,
1. How many maximum instances of Display are supported currently?
Above is my doubts because in vision_sdk/links_fw/include/link_api/displayLink.h file,
DisplayLink_displayID enum is for maximum 4 instances.
2. Can we increase/decrease that number ?
Also in vision_sdk/links_fw/src/rtos/links_ipu/display/displayLink_priv.h file maximum display link instances supported is 4 count,
#define DISPLAY_LINK_OBJ_MAX (4U)
Guide for the same.
Regards,
Kajal