Tool/software: Linux
Hello, I have got an issue with Linux 4.4.84 from PSDK 3.03 running on TDA2xx EVA board.
I have noticed that the accesses to PCI configuration space registers are not aligned to 4B boundary which results in incorrect reading of the, for example, status register. Upon implementing the accesses using pci_bus_read_config_dword they are being read correctly.
Thinking that this is a problem related solely to the Linux version, I've had a look into the same code from more recent kernels and it is the same. However, on my PC where I run kernel 4.16.7 all my PCI devices' registers are correctly read using those non-aligned accesses.
What I would like to ask is if this problem is in any way related to the board itself and its A15 core. I'm seeing much more non-aligned accesses which probably need to be patched. Is this a known problem when it comes to TI boards? If yes, is there any official patch for this?
Thank you in advance.
Nick