Part Number: TDA2EXEVM
Hi TIDL experts,
I use TIDL.01.01.02.00.
I have a modified jacinto SSD model with a lot of detector head.(10 heads)
It can not work properly on the usecase. it stuck and i even can not see the statistic.
IPU1-0] 16.372079 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023
[IPU1-0] 16.372201 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 262144 B (256 KB), Free size = 243176 B (237 KB)
[IPU1-0] 16.372354 s: SYSTEM: Heap = SR_OCMC @ 0x00000000, Total size = 0 B (0 KB), Free size = 0 B (0 KB)
[IPU1-0] 16.372506 s: SYSTEM: Heap = SR_DDR_CACHED @ 0x89c03000, Total size = 368037888 B (350 MB), Free size = 239153152 B (228 MB)
[IPU1-0] 16.372689 s: SYSTEM: Heap = SR_DDR_NON_CACHED @ 0xbfb00000, Total size = 127360 B (0 MB), Free size = 92800 B (0 MB)
[IPU1-1] 16.373055 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023
[IPU1-1] 16.373177 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 655360 B (640 KB), Free size = 643368 B (628 KB)
[HOST ] 16.373543 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023
[HOST ] 16.373543 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 6291456 B (6144 KB), Free size = 6236464 B (6090 KB)
And i do some experiment on the model, i try to reduce the heads of the model.(start removing from the top)
It works at 8 heads eventually. and the FPS is 24 .
But it can not work if the number of heads is bigger than 9.
Is there any possible reason about it?
it should not drop from 24 to 0 FPS?
I use model import trace dump on the model , and the reuslts is proper.
I do not have debugger so i can not use testbench.
I am looking forward to your answer.
Thank you so much.
Best Regards,
Jason