Other Parts Discussed in Thread: AM5728
Tool/software: TI-RTOS
Hello, I'm using AM572x IDK board, TI-RTOS SDK 05.01.00.11 and timeSync example.
I want to use pruss 2 port 1 (PRU2 ETH1 tag on board) as a PTP slave timeSync port in DualMac mode. But when I run your example, only PRU2.0 (PRU2 ETH0 tag on board) is working as a PTP source port.
I'm understand, that I can use only one PTP source for 2 PRU ports, but what do I need to change in example project to sync PTP only by PRU2.1 port?
P.S. I'm trying to change TIMESYNC_EXAMPLE_TEST_PORT0 define to 0 in src/example.h and it disables PRU2.0 sync, but doesn't enable PRU2.1 sync.
P.P.S. I'm using Ubuntu 16.04.5 LTS x64, TI-RTOS SDK v05.01.00.11, CCS v8.2.0