Tool/software: Linux
Hi,
I'm working on AM5728 EVM.
In our project we prefer to connect the EVM's USB (2.0 / 3.0) to Application Processor's (mangOH Red- WP) USB Host with an OTG Cable
In order to transfer the data from USB device(EVM) to USB Host(mangOH Red) we want to make above connection.
In AM5728 sdk many USB folders are available, but I'm not able to relate which USB.h and USB.c files are used for my project.
Suggest me with the appropriate USB.h or USB.c files path in the sdk-linux-am57xx-evm-05.00.00.15.
Regards,
GAG.