Tool/software: Linux
Champs,
Customer requires to put PRU Ethernet port into a test mode where all Rx traffic is looped back into Tx directly without FW/SW involvement (for pure HW data path verification purpose). The autoforward mode described in paragraph 30.1.9.2.1.1 seem to be the right tool for the job however there are two questions:
1. From PRU Ethernet driver description it is not clear if it supports putting port in this mode at all.
2. I can not find anywhere in the TRM how to enable this mode. RX_AUTO_FWD_PRE bit seems to only enable preamble forwarding not the whole packet.
Basically what they want to do is something similar to CPSW FIFO loopback (paragraph 24.11.4.8.13 in TRM). Is this at all possible?
Thanks
Michael