This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Change EMIF clock speed at Linux side



Hi,

   I have been told that maximum frequency for EMIF is fixed  - 100 MHz. at 1.0 V instead of 75 MHz

   By look around the TI power management code, I found the following definition and believe this is where the 100 MHz is defined.

   Can someone confirm this?

   Also, if I want to modify the default EMIF frequency to 90MHz, is this the only line needs to be edited? Any caution I have to take?

 ./arch/arm/mach-davinci/da850.c

 static struct davinci_cpufreq_config cpufreq_info = {

                .freq_table = &da850_freq_table[0],

#ifdef CONFIG_REGULATOR

                .init = da850_regulator_init,

                .set_voltage = da850_set_voltage,

#endif

               .asyncrate = 100000000,

};

regards,

Francis