This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AIS and AISgen

Hi Jeff,

From "Using the OMAP-L1x8 Bootloader Application Report" document, AIS seems can totally replace the functionality of UBL. So, it is a matter of choice whether to use AIS or UBL.

The advantage of using UBL is I have the source code, and I can easily enhance it to add addtional features.

But, AIS seems to provide the mechanisme to extend its functionality using Jump command (0x58535905). Any example that I can take a look on this mechanisme ?

What I am trying to do here is before AIS loads image from boot device, I want it to prompt user to select the image, let say I have 3 different images on the boot device.

I want this Jump command to return the user selection to bootloader, so that bootloader can continue to load the user selected image.

Can I achieve this by using AIS ?

rgds,

kc Wong