Part Number: AM5728
Tool/software: Linux
Hi,
I m using attached create-sdcard.sh script file. Using 8gb sd card.
I m having 16gb ti evm sd card also in which starting address is 63
Device Boot Start End Sectors Size Id Type
/dev/sdb1 * 63 144584 144522 70.6M b W95 FAT32
/dev/sdb2 144585 4964084 4819500 2.3G 83 Linux
/dev/sdb3 4964085 30925124 25961040 12.4G 83 Linux
My sd card default starting address is 2048. I want to use own sd card and images.
While using script file .,
################################################################################
Partitioning Boot
################################################################################
mkfs.fat 3.0.28 (2015-05-16)
mkfs.fat: warning - lowercase labels might not work properly with DOS or Windows
/dev/sdb1: No such file or directory
################################################################################
Partitioning rootfs
################################################################################
mke2fs 1.42.13 (17-May-2015)
The file /dev/sdb2 does not exist and no size was specified.
################################################################################
Partitioning is now done
Continue to install filesystem or select 'n' to safe exit
**Warning** Continuing will erase files any files in the partitions
################################################################################
I tried partitioning the sd card manually, but the evm board itself is not booting.
Can you please provide me the specific create-sdcard.sh script.
and also some input regarding this starting address of SD card.
Please provide me the guidance to partition the sd card.