Part Number: PROCESSOR-SDK-OMAPL138
Other Parts Discussed in Thread: OMAPL138
Tool/software: TI-RTOS
Hi All,
I am working on omapl138 C674 and using pdk_omapl138_1_0_5. Currently, I am facing an issue with spi interrupt.
So, I am trying it in loopback mode. When ever I am trying to transfer more than 1byte, control is getting stuck in last byte to receive i.e., receive count is 1 but transmit count is 0. When I stop it in debug mode and make transmit count as 1, I am able to see tx data in rx buffer and control is coming out of the isr.
My spi configurations as follows...
SPI_socGetInitCfg(SPI_INSTANCE, &spi_cfg);
spi_cfg.enableIntr = true;
SPI_socSetInitCfg(SPI_INSTANCE, &spi_cfg);
SPI_Params_init(&spiParams);
SPI_init();
hwHandle = (SPI_Handle)SPI_open(SPI_INSTANCE, &spiParams);
SPI_control(hwHandle,SPI_V0_CMD_LOOPBACK,(void *) &loop);
if (!hwHandle)
{
testPassed = false;
while(1);
}
Task_sleep(1000);
/* Enable transfer */
xferEnable = 1;
SPI_control(hwHandle, SPI_V0_CMD_XFER_ACTIVATE, (void *)&xferEnable);
Then I start with transaction.
Can anyone help me to comeout off this problem?
Thanks...