This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2: TIDL SSD MODEL

Part Number: TDA2


hi,

       Could you please share me with the TIDL ssd model formated as text t which can be imported into caffe framework and run normally ? As you can see the picture below,there is only the binary format of the ssd model and parameter, where is the text format of these two files ?  Which files at the web link "https://github.com/tidsp/caffe-jacinto/tree/caffe-0.17/models/VGGNet/coco/SSD_300x300"

        I mean the two files "tidl_net_jdetNet_ssd.bin tidl_param_jdetNet_ssd.bin". Could we think of tidl_param_jdetNet_ssd.bin as caffemodel format file and the tidl_net_jdetNet_ssd.bin as prototxt file which shows the structure of the ssd net model?

Best,