Tool/software: Linux
==== netstat -s ===== Ip: 139961 total packets received 0 forwarded 0 incoming packets discarded 139953 incoming packets delivered 150475 requests sent out Icmp: 0 ICMP messages received 0 input ICMP message failed. ICMP input histogram: 0 ICMP messages sent 0 ICMP messages failed ICMP output histogram: Tcp: 6 active connections openings 0 passive connection openings 0 failed connection attempts 0 connection resets received 1 connections established 107497 segments received 117975 segments send out 0 segments retransmited 0 bad segments received. 0 resets sent Udp: 32440 packets received 0 packets to unknown port received. 0 packet receive errors 32487 packets sent UdpLite: TcpExt: 4 TCP sockets finished time wait in fast timer 709 delayed acks sent 7 packets directly queued to recvmsg prequeue. 228 bytes directly received in process context from prequeue 93014 packet headers predicted 6 packets header predicted and directly queued to user 154 acknowledgments not containing data payload received 66796 predicted acknowledgments TCPLossProbes: 26 TCPLossProbeRecovery: 17 17 DSACKs received TCPDSACKIgnoredNoUndo: 16 IpExt: InNoRoutes: 8 InBcastPkts: 16 InOctets: 51680282 OutOctets: 25409100 InBcastOctets: 5248 ==== snmp ==== Ip: Forwarding DefaultTTL InReceives InHdrErrors InAddrErrors ForwDatagrams InUnknownProtos InDiscards InDelivers OutRequests OutDiscards OutNoRoutes ReasmTimeout ReasmReqds ReasmOKs ReasmFails FragOKs FragFails FragCreates Ip: 2 64 139967 0 0 0 0 0 139959 150481 0 0 0 0 0 0 0 0 0 Icmp: InMsgs InErrors InCsumErrors InDestUnreachs InTimeExcds InParmProbs InSrcQuenchs InRedirects InEchos InEchoReps InTimestamps InTimestampReps InAddrMasks InAddrMaskReps OutMsgs OutErrors OutDestUnreachs OutTimeExcds OutParmProbs OutSrcQuenchs OutRedirects OutEchos OutEchoReps OutTimestamps OutTimestampReps OutAddrMasks OutAddrMaskReps Icmp: 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 Tcp: RtoAlgorithm RtoMin RtoMax MaxConn ActiveOpens PassiveOpens AttemptFails EstabResets CurrEstab InSegs OutSegs RetransSegs InErrs OutRsts InCsumErrors Tcp: 1 200 120000 -1 6 0 0 0 1 107503 117981 0 0 0 0 Udp: InDatagrams NoPorts InErrors OutDatagrams RcvbufErrors SndbufErrors InCsumErrors Udp: 32440 0 0 32487 0 0 0 UdpLite: InDatagrams NoPorts InErrors OutDatagrams RcvbufErrors SndbufErrors InCsumErrors UdpLite: 0 0 0 0 0 0 0 ==== net dev ==== Inter-| Receive | Transmit face |bytes packets errs drop fifo frame compressed multicast|bytes packets errs drop fifo colls carrier compressed eth1.bp_00_lo: 336 6 0 0 0 0 0 0 132 6 0 0 0 0 0 0 eth1.bp_00: 252 6 0 0 0 0 0 0 132 6 0 0 0 0 0 0 eth1.inm_01: 167896176 3997528 0 47 0 0 0 3997528 0 0 0 0 0 0 0 0 eth1.inm_00: 167855310 3996555 0 47 0 0 0 3996555 0 0 0 0 0 0 0 0 eth1.bp_01: 3123172 34274 0 0 0 0 0 0 9235974 34282 0 0 0 0 0 0 eth1.bp_02: 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 eth2.dbg_00: 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 lo: 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 eth1.dct_01: 248812 1348 0 0 0 0 0 0 256722 1341 0 0 0 0 0 0 eth1.dct_00: 14539960 330964 0 0 0 0 0 0 256134 1327 0 0 0 0 0 0 eth0: 67854090 409080 0 4 0 0 0 0 18013738 119325 0 0 0 0 0 0 eth1: 504155832 8360675 0 0 0 0 0 0 10521254 60974 0 0 0 0 0 0 eth2: 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 eth1.bp_02_lo: 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 eth1.bp_01_lo: 3296 38 0 0 0 0 0 38 0 0 0 0 0 0 0 0 ==== udp ==== sl local_address rem_address st tx_queue rx_queue tr tm->when retrnsmt uid timeout inode ref pointer drops 24: B2FDA8C0:2718 00000000:0000 07 00000000:00000000 00:00000000 00000000 0 0 9729 2 9d928300 0 69: 00000000:0045 00000000:0000 07 00000000:00000000 00:00000000 00000000 0 0 9763 2 9d928f00 0 162: 00000000:3AA2 00000000:0000 07 00000000:00000000 00:00000000 00000000 0 0 9779 2 9d928c00 0 169: 00000000:3AA9 00000000:0000 07 00000000:00000000 00:00000000 00000000 0 0 9806 2 9d928000 0 185: B2FDA8C0:36B9 00000000:0000 07 00000000:00000000 00:00000000 00000000 0 0 9724 2 9d928900 0 228: B2FDA8C0:2EE4 00000000:0000 07 00000000:00000000 00:00000000 00000000 0 0 9725 2 9d928600 0 ==== ifconfig ==== eth0 Link encap:Ethernet HWaddr 98:84:e3:5b:3b:cf inet addr:192.168.253.11 Bcast:192.168.253.15 Mask:255.255.255.248 UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:409091 errors:0 dropped:4 overruns:0 frame:0 TX packets:119336 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:67855916 (64.7 MiB) TX bytes:18015696 (17.1 MiB) eth1 Link encap:Ethernet HWaddr d8:ef:cd:b3:96:82 UP BROADCAST RUNNING MULTICAST MTU:2000 Metric:1 RX packets:8360678 errors:0 dropped:0 overruns:0 frame:0 TX packets:60974 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:504156012 (480.8 MiB) TX bytes:10521254 (10.0 MiB) eth2 Link encap:Ethernet HWaddr 02:40:43:77:0a:31 UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B) eth1.bp_00 Link encap:Ethernet HWaddr d8:ef:cd:b3:96:82 UP BROADCAST RUNNING MULTICAST MTU:2000 Metric:1 RX packets:6 errors:0 dropped:0 overruns:0 frame:0 TX packets:6 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:0 RX bytes:252 (252.0 B) TX bytes:132 (132.0 B) eth1.bp_01 Link encap:Ethernet HWaddr d8:ef:cd:b3:96:82 inet addr:192.168.253.178 Bcast:192.168.253.255 Mask:255.255.255.0 UP BROADCAST RUNNING MULTICAST MTU:2000 Metric:1 RX packets:34274 errors:0 dropped:0 overruns:0 frame:0 TX packets:34282 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:0 RX bytes:3123172 (2.9 MiB) TX bytes:9235974 (8.8 MiB) eth1.bp_02 Link encap:Ethernet HWaddr d8:ef:cd:b3:96:82 UP BROADCAST RUNNING MULTICAST MTU:2000 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:0 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B) eth1.bp_00_lo Link encap:Ethernet HWaddr 02:40:43:77:0a:30 UP BROADCAST RUNNING MULTICAST MTU:2000 Metric:1 RX packets:6 errors:0 dropped:0 overruns:0 frame:0 TX packets:6 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:0 RX bytes:336 (336.0 B) TX bytes:132 (132.0 B) eth1.bp_01_lo Link encap:Ethernet HWaddr 02:40:43:77:0a:30 UP BROADCAST RUNNING MULTICAST MTU:2000 Metric:1 RX packets:38 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:0 RX bytes:3296 (3.2 KiB) TX bytes:0 (0.0 B) eth1.bp_02_lo Link encap:Ethernet HWaddr 02:40:43:77:0a:30 UP BROADCAST RUNNING MULTICAST MTU:2000 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:0 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B) eth1.dct_00 Link encap:Ethernet HWaddr d8:ef:cd:b3:96:82 inet addr:192.168.129.92 Bcast:192.168.129.255 Mask:255.255.255.0 UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:330965 errors:0 dropped:0 overruns:0 frame:0 TX packets:1327 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:0 RX bytes:14540002 (13.8 MiB) TX bytes:256134 (250.1 KiB) eth1.dct_01 Link encap:Ethernet HWaddr d8:ef:cd:b3:96:82 inet addr:192.168.130.92 Bcast:192.168.130.255 Mask:255.255.255.0 UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:1348 errors:0 dropped:0 overruns:0 frame:0 TX packets:1341 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:0 RX bytes:248812 (242.9 KiB) TX bytes:256722 (250.7 KiB) eth1.inm_00 Link encap:Ethernet HWaddr d8:ef:cd:b3:96:82 UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:3996556 errors:0 dropped:47 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:0 RX bytes:167855352 (160.0 MiB) TX bytes:0 (0.0 B) eth1.inm_01 Link encap:Ethernet HWaddr d8:ef:cd:b3:96:82 UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:3997529 errors:0 dropped:47 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:0 RX bytes:167896218 (160.1 MiB) TX bytes:0 (0.0 B) eth2.dbg_00 Link encap:Ethernet HWaddr 02:40:43:77:0a:31 inet addr:192.168.131.92 Bcast:192.168.131.255 Mask:255.255.255.0 UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:0 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B) lo Link encap:Local Loopback inet addr:127.0.0.1 Mask:255.0.0.0 UP LOOPBACK RUNNING MTU:65536 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:0 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B) 2018-11-29 03:12:27.%N PCS-R module Register devmem 0x02F00600 0x00000000 devmem 0x02F00604 0x00000000 devmem 0x02F00608 0x00000000 devmem 0x02F0060C 0x40000000 devmem 0x02F00610 0x00000000 devmem 0x02F00614 0x00000000 devmem 0x02F00618 0x00000000 devmem 0x02F0061C 0x00000000 devmem 0x02F00620 0x00000000 devmem 0x02F00624 0x00000000 devmem 0x02F00628 0x00000000 devmem 0x02F0062C 0x00000000 10GbE switch info devmem 0x02F01000 0x4EE30101 devmem 0x02F01004 0x00000004 devmem 0x02F01008 0x00000000 devmem 0x02F0100C 0x00000007 devmem 0x02F01010 0x00000000 devmem 0x02F01014 0x00000000 devmem 0x02F01018 0x00003003 devmem 0x02F0101C 0x0000000B devmem 0x02F01020 0x00000008 devmem 0x02F01024 0x00000007 devmem 0x02F01028 0x00000113 devmem 0x02F01034 0x00000202 devmem 0x02F01038 0x00000000 devmem 0x02F0103C 0x00000210 devmem 0x02F01040 0x00000201 devmem 0x02F01044 0x76543210 devmem 0x02F01048 0x00002520 devmem 0x0231FFE0 0xF0F9F03A devmem 0x02F00114 0x00000030 devmem 0x02F0165C 0x00000000 devmem 0x231EBF8 0x66030006 devmem 0x231E5C0 0x00000000 devmem 0x231FFE4 0xF0F9F03A devmem 0x231FFF4 0xFF380303 10G statistics devmem 0x02f01800 0x00000000 devmem 0x02f01804 0x00000000 devmem 0x02f0180c 0x00000000 devmem 0x02f01818 0x00000000 devmem 0x02f01828 0x00000000 devmem 0x02f0183c 0x00000002 devmem 0x02f01854 0x00000000 devmem 0x02f01870 0x00000000 devmem 0x02f01890 0x00000100 devmem 0x02f018b4 0x00000004 devmem 0x02f018dc 0x00000000 devmem 0x02f01908 0x00000004 devmem 0x02f01938 0x00000000 devmem 0x02f0196c 0x00000000 devmem 0x02f019a4 0x00000000 devmem 0x02f019e0 0x00000248 devmem 0x02f01a20 0x00000000 devmem 0x02f01a64 0x00000000 devmem 0x02f01aac 0x00000000 devmem 0x02f01af8 0x00000000 devmem 0x02f01b48 0x00000000 devmem 0x02f01b9c 0x00000000 devmem 0x02f01bf4 0x00000000 devmem 0x02f01c50 0x00000000 devmem 0x02f01cb0 0x00000000 devmem 0x02f01d14 0x00000000 devmem 0x02f01d7c 0x00000000 devmem 0x02f01de8 0x00000000 devmem 0x02f01e58 0x00000000 devmem 0x02f01ecc 0x00000000 devmem 0x02f01f44 0x00000000 devmem 0x02f01fc0 0x00000000 devmem 0x02f02040 0x00000000 devmem 0x02f020c4 0x00000000 devmem 0x02f0214c 0x00000000 devmem 0x02f021d8 0x00000000 devmem 0x02f02268 0x00000000 devmem 0x02f022fc 0x00000000 devmem 0x02f02394 0x00000000 devmem 0x02f02430 0x00000000 devmem 0x02f024d0 0x00000000 devmem 0x02f02574 0x00000000 devmem 0x02f0261c 0x00000000 devmem 0x02f026c8 0x00000000 devmem 0x02f02778 0x00000000 devmem 0x02f0282c 0x00000000 devmem 0x02f028e4 0x00000000 devmem 0x02f029a0 0x00000000 devmem 0x02f02a60 0x00000000 devmem 0x02f02b24 0x00000000 devmem 0x02f02bec 0x00000000 devmem 0x02f02cb8 0x00000000 devmem 0x02f02d88 0x00000000 devmem 0x02f02e5c 0x00000000 devmem 0x02f02f34 0x00000000 devmem 0x02f03010 0x00000000 devmem 0x02f030f0 0x00000000 devmem 0x02f031d4 0x00000000 devmem 0x02f032bc 0x00000000 devmem 0x02f033a8 0x00000000 devmem 0x02f03498 0x00000000 devmem 0x02f0358c 0x00000000 devmem 0x02f03684 0x00000000 devmem 0x02f03780 0x00000000 devmem 0x02f03880 0x00000000 devmem 0x02f03984 0x00000000 devmem 0x02f03a8c 0x00000000 devmem 0x02f03b98 0x00000000 devmem 0x02f03ca8 0x00000000 devmem 0x02f03dbc 0x00000000 devmem 0x02f03ed4 0x00000000 devmem 0x02f03ff0 0x00000000 devmem 0x02f04110 0x00000000 devmem 0x02f04234 0x00000000 devmem 0x02f0435c 0x00000000 devmem 0x02f04488 0x00000000 devmem 0x02f045b8 0x00000000 devmem 0x02f046ec 0x00000000 devmem 0x02f04824 0x00000000 devmem 0x02f04960 0x00000000 devmem 0x02f04aa0 0x00000000 devmem 0x02f04be4 0x00000000 devmem 0x02f04d2c 0x00000000 devmem 0x02f04e78 0x00000000 devmem 0x02f04fc8 0x00000000 devmem 0x02f0511c 0x00000000 devmem 0x02f05274 0x00000000 devmem 0x02f053d0 0x00000000 devmem 0x02f05530 0x00000000 devmem 0x02f05694 0x00000000 devmem 0x02f057fc 0x00000000 devmem 0x02f05968 0x00000000 devmem 0x02f05ad8 0x00000000 devmem 0x02f05c4c 0x00000000 devmem 0x02f05dc4 0x00000000 devmem 0x02f05f40 0x00000000 devmem 0x02f060c0 0x00000000 devmem 0x02f06244 0x00000000 devmem 0x02f063cc 0x00000000 devmem 0x02f06558 0x00000000 devmem 0x02f066e8 0x00000000 devmem 0x02f0687c 0x00000000 devmem 0x02f06a14 0x00000000 devmem 0x02f06bb0 0x00000000 devmem 0x02f06d50 0x00000000 devmem 0x02f06ef4 0x00000000 devmem 0x02f0709c 0x00000000 devmem 0x02f07248 0x00000000 devmem 0x02f073f8 0x00000000 devmem 0x02f075ac 0x00000000 devmem 0x02f07764 0x00000000 devmem 0x02f07920 0x00000000 devmem 0x02f07ae0 0x00000000 devmem 0x02f07ca4 0x00000000 devmem 0x02f07e6c 0x00000000 devmem 0x02f08038 0x00000000 devmem 0x02f08208 0x00000000 devmem 0x02f083dc 0x00000000 devmem 0x02f085b4 0x00000000 devmem 0x02f08790 0x00000000 devmem 0x02f08970 0x00000000 devmem 0x02f08b54 0x00000000 devmem 0x02f08d3c 0x00000000 devmem 0x02f08f28 0x00000000 devmem 0x02f09118 0x00000000 devmem 0x02f0930c 0x00000000 devmem 0x02f09504 0x00000000 devmem 0x02f09700 0x00000000 devmem 0x02f09900 0x00000000 devmem 0x02f09b04 0x00000000 devmem 0x02f09d0c 0x00000000 devmem 0x02f09f18 0x00000000 devmem 0x02f0a128 0x00000000 devmem 0x02f0a33c 0x00000000 devmem 0x02f0a554 0x00000000 devmem 0x02f0a770 0x00000000 devmem 0x02f0a990 0x00000000 devmem 0x02f0abb4 0x00000000 devmem 0x02f0addc 0x00000000 devmem 0x02f0b008 0x00000000 devmem 0x02f0b238 0x00000000 devmem 0x02f0b46c 0x00000000 devmem 0x02f0b6a4 0x00000000 devmem 0x02f0b8e0 0x00000000 devmem 0x02f0bb20 0x00000000 devmem 0x02f0bd64 0x00000000 devmem 0x02f0bfac 0x00000000 devmem 0x02f0c1f8 0x00000000 devmem 0x02f0c448 0x00000000 devmem 0x02f0c69c 0x00000000 devmem 0x02f0c8f4 0x00000000 devmem 0x02f0cb50 0x00000000 devmem 0x02f0cdb0 0x00000000 devmem 0x02f0d014 0x00000000 devmem 0x02f0d27c 0x00000000 devmem 0x02f0d4e8 0x00000000 devmem 0x02f0d758 0x00000000 devmem 0x02f0d9cc 0x00000000 devmem 0x02f0dc44 0x00000000 devmem 0x02f0dec0 0x00000000 devmem 0x02f0e140 0x00000000 devmem 0x02f0e3c4 0x00000000 devmem 0x02f0e64c 0x00000000 devmem 0x02f0e8d8 0x00000000
Now K2 can not receive messages when communicating with AXM. XFI0 of K2 connects with AXM HSS3-2. K2 suddenly appears in the working process that K2 can not receive messages, but K2 can send messages to AXM. Has K2 ever had this problem?
Attached are some register information for K2. Cloud you check the K2 registers logs? If these registers are not enough, do you need to add other registers? If additional register logs are needed, could you give the registers address that needs to be added? May I have your telephone number? Thanks.