This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3352: RAM test at uboot taking lot of time

Part Number: AM3352

Tool/software: Linux

I want to test whole RAM using mtest command from u-boot.

Below command I am using in u-boot.

=> mtest

Testing 80000000 ... 8fffffff:
Pattern 00000000 Writing...

It is taking around 3 to 4 hours to test.

Beaglebone green wireless I am using, Is there anything I am missing?

Can you help me any workaround to reduce time?

I tried to test RAM in kernel level using memtest=2 It is very fast and it is taking only few seconds, same thing I am looking in u-boot level. 

  

  • Hi Dheeraj,

    Are you using Processor SDK and if it is true could you specify the version?
    Also which version is u-boot?
    Could you attach u-boot defconfig file?

    Regards,
    Tsvetolin Shulev
  • #
    # Automatically generated file; DO NOT EDIT.
    # U-Boot 2016.03 Configuration
    #
    CONFIG_CREATE_ARCH_SYMLINK=y
    CONFIG_HAVE_GENERIC_BOARD=y
    CONFIG_SYS_GENERIC_BOARD=y
    # CONFIG_ARC is not set
    CONFIG_ARM=y
    # CONFIG_AVR32 is not set
    # CONFIG_BLACKFIN is not set
    # CONFIG_M68K is not set
    # CONFIG_MICROBLAZE is not set
    # CONFIG_MIPS is not set
    # CONFIG_NDS32 is not set
    # CONFIG_NIOS2 is not set
    # CONFIG_OPENRISC is not set
    # CONFIG_PPC is not set
    # CONFIG_SANDBOX is not set
    # CONFIG_SH is not set
    # CONFIG_SPARC is not set
    # CONFIG_X86 is not set
    CONFIG_SYS_ARCH="arm"
    CONFIG_SYS_CPU="armv7"
    CONFIG_SYS_SOC="am33xx"
    CONFIG_SYS_VENDOR="ti"
    CONFIG_SYS_BOARD="am335x"
    CONFIG_SYS_CONFIG_NAME="am335x_evm"
    
    #
    # ARM architecture
    #
    CONFIG_HAS_VBAR=y
    CONFIG_HAS_THUMB2=y
    CONFIG_CPU_V7=y
    # CONFIG_SEMIHOSTING is not set
    # CONFIG_SYS_L2CACHE_OFF is not set
    # CONFIG_ARCH_AT91 is not set
    # CONFIG_TARGET_EDB93XX is not set
    # CONFIG_TARGET_VCMA9 is not set
    # CONFIG_TARGET_SMDK2410 is not set
    # CONFIG_TARGET_ASPENITE is not set
    # CONFIG_TARGET_GPLUGD is not set
    # CONFIG_ARCH_DAVINCI is not set
    # CONFIG_KIRKWOOD is not set
    # CONFIG_ARCH_MVEBU is not set
    # CONFIG_TARGET_DEVKIT3250 is not set
    # CONFIG_TARGET_WORK_92105 is not set
    # CONFIG_TARGET_MX25PDK is not set
    # CONFIG_TARGET_ZMX25 is not set
    # CONFIG_TARGET_APF27 is not set
    # CONFIG_TARGET_APX4DEVKIT is not set
    # CONFIG_TARGET_XFI3 is not set
    # CONFIG_TARGET_M28EVK is not set
    # CONFIG_TARGET_MX23EVK is not set
    # CONFIG_TARGET_MX28EVK is not set
    # CONFIG_TARGET_MX23_OLINUXINO is not set
    # CONFIG_TARGET_BG0900 is not set
    # CONFIG_TARGET_SANSA_FUZE_PLUS is not set
    # CONFIG_TARGET_SC_SPS_1 is not set
    # CONFIG_ORION5X is not set
    # CONFIG_TARGET_SPEAR300 is not set
    # CONFIG_TARGET_SPEAR310 is not set
    # CONFIG_TARGET_SPEAR320 is not set
    # CONFIG_TARGET_SPEAR600 is not set
    # CONFIG_TARGET_STV0991 is not set
    # CONFIG_TARGET_X600 is not set
    # CONFIG_TARGET_IMX31_PHYCORE is not set
    # CONFIG_TARGET_MX31ADS is not set
    # CONFIG_TARGET_MX31PDK is not set
    # CONFIG_TARGET_WOODBURN is not set
    # CONFIG_TARGET_WOODBURN_SD is not set
    # CONFIG_TARGET_FLEA3 is not set
    # CONFIG_TARGET_MX35PDK is not set
    # CONFIG_ARCH_BCM283X is not set
    # CONFIG_TARGET_VEXPRESS_CA15_TC2 is not set
    # CONFIG_TARGET_VEXPRESS_CA5X2 is not set
    # CONFIG_TARGET_VEXPRESS_CA9X4 is not set
    # CONFIG_TARGET_KWB is not set
    # CONFIG_TARGET_TSERIES is not set
    # CONFIG_TARGET_CM_T335 is not set
    # CONFIG_TARGET_PEPPER is not set
    # CONFIG_TARGET_AM335X_IGEP0033 is not set
    # CONFIG_TARGET_PCM051 is not set
    # CONFIG_TARGET_DRACO is not set
    # CONFIG_TARGET_THUBAN is not set
    # CONFIG_TARGET_RASTABAN is not set
    # CONFIG_TARGET_PXM2 is not set
    # CONFIG_TARGET_RUT is not set
    # CONFIG_TARGET_PENGWYN is not set
    # CONFIG_TARGET_AM335X_BALTOS is not set
    CONFIG_TARGET_AM335X_EVM=y
    # CONFIG_TARGET_AM335X_SL50 is not set
    # CONFIG_TARGET_AM43XX_EVM is not set
    # CONFIG_TARGET_BAV335X is not set
    # CONFIG_TARGET_TI814X_EVM is not set
    # CONFIG_TARGET_TI816X_EVM is not set
    # CONFIG_TARGET_BCM28155_AP is not set
    # CONFIG_TARGET_BCMCYGNUS is not set
    # CONFIG_TARGET_BCMNSP is not set
    # CONFIG_ARCH_EXYNOS is not set
    # CONFIG_ARCH_S5PC1XX is not set
    # CONFIG_ARCH_HIGHBANK is not set
    # CONFIG_ARCH_INTEGRATOR is not set
    # CONFIG_ARCH_KEYSTONE is not set
    # CONFIG_ARCH_MX7 is not set
    # CONFIG_ARCH_MX6 is not set
    # CONFIG_ARCH_MX5 is not set
    # CONFIG_TARGET_M53EVK is not set
    # CONFIG_TARGET_MX51EVK is not set
    # CONFIG_TARGET_MX53ARD is not set
    # CONFIG_TARGET_MX53EVK is not set
    # CONFIG_TARGET_MX53LOCO is not set
    # CONFIG_TARGET_MX53SMD is not set
    # CONFIG_OMAP34XX is not set
    # CONFIG_OMAP44XX is not set
    # CONFIG_OMAP54XX is not set
    # CONFIG_RMOBILE is not set
    # CONFIG_ARCH_SOCFPGA is not set
    # CONFIG_TARGET_CM_T43 is not set
    # CONFIG_ARCH_SUNXI is not set
    # CONFIG_TARGET_TS4800 is not set
    # CONFIG_TARGET_VF610TWR is not set
    # CONFIG_TARGET_COLIBRI_VF is not set
    # CONFIG_TARGET_PCM052 is not set
    # CONFIG_ARCH_ZYNQ is not set
    # CONFIG_ARCH_ZYNQMP is not set
    # CONFIG_TEGRA is not set
    # CONFIG_TARGET_VEXPRESS64_AEMV8A is not set
    # CONFIG_TARGET_VEXPRESS64_BASE_FVP is not set
    # CONFIG_TARGET_VEXPRESS64_BASE_FVP_DRAM is not set
    # CONFIG_TARGET_VEXPRESS64_JUNO is not set
    # CONFIG_TARGET_LS2080A_EMU is not set
    # CONFIG_TARGET_LS2080A_SIMU is not set
    # CONFIG_TARGET_LS2080AQDS is not set
    # CONFIG_TARGET_LS2080ARDB is not set
    # CONFIG_TARGET_HIKEY is not set
    # CONFIG_TARGET_LS1021AQDS is not set
    # CONFIG_TARGET_LS1021ATWR is not set
    # CONFIG_TARGET_LS1043AQDS is not set
    # CONFIG_TARGET_LS1043ARDB is not set
    # CONFIG_TARGET_H2200 is not set
    # CONFIG_TARGET_COLIBRI_PXA270 is not set
    # CONFIG_ARCH_UNIPHIER is not set
    # CONFIG_STM32 is not set
    # CONFIG_ARCH_ROCKCHIP is not set
    # CONFIG_TARGET_THUNDERX_88XX is not set
    CONFIG_SYS_MALLOC_F_LEN=0x400
    CONFIG_CONS_INDEX=1
    CONFIG_SYS_MALLOC_F=y
    # CONFIG_SPL_SYS_MALLOC_SIMPLE is not set
    # CONFIG_SPL_DM is not set
    CONFIG_DM_SERIAL=y
    # CONFIG_DM_SPI is not set
    # CONFIG_DM_I2C is not set
    CONFIG_DM_GPIO=y
    CONFIG_SPL_STACK_R_ADDR=0x82000000
    # CONFIG_NOR is not set
    
    #
    # ARM debug
    #
    # CONFIG_DEBUG_LL is not set
    # CONFIG_DM_KEYBOARD is not set
    CONFIG_DEFAULT_DEVICE_TREE=""
    
    #
    # General setup
    #
    CONFIG_LOCALVERSION=""
    CONFIG_LOCALVERSION_AUTO=y
    CONFIG_CC_OPTIMIZE_FOR_SIZE=y
    CONFIG_EXPERT=y
    CONFIG_SYS_MALLOC_CLEAR_ON_INIT=y
    
    #
    # Boot images
    #
    CONFIG_SUPPORT_SPL=y
    CONFIG_SPL=y
    CONFIG_SPL_STACK_R=y
    # CONFIG_SPL_SEPARATE_BSS is not set
    # CONFIG_FIT is not set
    CONFIG_SYS_EXTRA_OPTIONS="NAND"
    
    #
    # Boot timing
    #
    # CONFIG_BOOTSTAGE is not set
    CONFIG_BOOTSTAGE_USER_COUNT=20
    CONFIG_BOOTSTAGE_STASH_ADDR=0
    CONFIG_BOOTSTAGE_STASH_SIZE=4096
    # CONFIG_CONSOLE_RECORD is not set
    
    #
    # Command line interface
    #
    # CONFIG_HUSH_PARSER is not set
    CONFIG_SYS_PROMPT="=> "
    
    #
    # Autoboot options
    #
    CONFIG_AUTOBOOT_KEYED=y
    CONFIG_AUTOBOOT_PROMPT="Press SPACE to abort autoboot in %d seconds\n"
    # CONFIG_AUTOBOOT_ENCRYPTION is not set
    CONFIG_AUTOBOOT_DELAY_STR="d"
    CONFIG_AUTOBOOT_STOP_STR=" "
    # CONFIG_AUTOBOOT_KEYED_CTRLC is not set
    
    #
    # Commands
    #
    
    #
    # Info commands
    #
    CONFIG_CMD_BDI=y
    CONFIG_CMD_CONSOLE=y
    # CONFIG_CMD_CPU is not set
    # CONFIG_CMD_LICENSE is not set
    
    #
    # Boot commands
    #
    CONFIG_CMD_BOOTD=y
    CONFIG_CMD_BOOTM=y
    CONFIG_CMD_ELF=y
    CONFIG_CMD_GO=y
    CONFIG_CMD_RUN=y
    CONFIG_CMD_IMI=y
    # CONFIG_CMD_IMLS is not set
    CONFIG_CMD_XIMG=y
    
    #
    # Environment commands
    #
    CONFIG_CMD_EXPORTENV=y
    CONFIG_CMD_IMPORTENV=y
    CONFIG_CMD_EDITENV=y
    CONFIG_CMD_SAVEENV=y
    CONFIG_CMD_ENV_EXISTS=y
    
    #
    # Memory commands
    #
    CONFIG_CMD_MEMORY=y
    CONFIG_CMD_CRC32=y
    CONFIG_LOOPW=y
    CONFIG_CMD_MEMTEST=y
    CONFIG_CMD_MX_CYCLIC=y
    CONFIG_CMD_MEMINFO=y
    
    #
    # Device access commands
    #
    CONFIG_CMD_DM=y
    # CONFIG_CMD_DEMO is not set
    CONFIG_CMD_LOADB=y
    CONFIG_CMD_LOADS=y
    # CONFIG_CMD_FLASH is not set
    # CONFIG_CMD_NAND is not set
    # CONFIG_CMD_SF is not set
    # CONFIG_CMD_SPI is not set
    # CONFIG_CMD_I2C is not set
    # CONFIG_CMD_USB is not set
    CONFIG_CMD_FPGA=y
    CONFIG_CMD_GPIO=y
    
    #
    # Shell scripting commands
    #
    CONFIG_CMD_ECHO=y
    CONFIG_CMD_ITEST=y
    CONFIG_CMD_SOURCE=y
    CONFIG_CMD_SETEXPR=y
    
    #
    # Network commands
    #
    CONFIG_CMD_NET=y
    # CONFIG_CMD_TFTPPUT is not set
    # CONFIG_CMD_TFTPSRV is not set
    # CONFIG_CMD_RARP is not set
    # CONFIG_CMD_DHCP is not set
    CONFIG_CMD_NFS=y
    # CONFIG_CMD_PING is not set
    # CONFIG_CMD_CDP is not set
    # CONFIG_CMD_SNTP is not set
    # CONFIG_CMD_DNS is not set
    # CONFIG_CMD_LINK_LOCAL is not set
    
    #
    # Misc commands
    #
    # CONFIG_CMD_TIME is not set
    CONFIG_CMD_MISC=y
    # CONFIG_CMD_TIMER is not set
    
    #
    # Power commands
    #
    
    #
    # Security commands
    #
    CONFIG_SUPPORT_OF_CONTROL=y
    
    #
    # Device Tree Control
    #
    # CONFIG_OF_CONTROL is not set
    CONFIG_NET=y
    # CONFIG_NET_RANDOM_ETHADDR is not set
    # CONFIG_NETCONSOLE is not set
    CONFIG_NET_TFTP_VARS=y
    
    #
    # Device Drivers
    #
    
    #
    # Generic Driver Options
    #
    CONFIG_DM=y
    CONFIG_DM_WARN=y
    CONFIG_DM_DEVICE_REMOVE=y
    CONFIG_DM_STDIO=y
    CONFIG_DM_SEQ_ALIAS=y
    # CONFIG_SPL_DM_SEQ_ALIAS is not set
    # CONFIG_REGMAP is not set
    # CONFIG_SPL_REGMAP is not set
    # CONFIG_DEVRES is not set
    # CONFIG_ADC is not set
    # CONFIG_ADC_EXYNOS is not set
    # CONFIG_ADC_SANDBOX is not set
    CONFIG_DISK=y
    
    #
    # Clock
    #
    # CONFIG_CLK is not set
    # CONFIG_CPU is not set
    
    #
    # Hardware crypto devices
    #
    # CONFIG_FSL_CAAM is not set
    
    #
    # Demo for driver model
    #
    # CONFIG_DM_DEMO is not set
    
    #
    # DFU support
    #
    # CONFIG_DFU_TFTP is not set
    
    #
    # DMA Support
    #
    # CONFIG_DMA is not set
    # CONFIG_TI_EDMA3 is not set
    
    #
    # GPIO Support
    #
    # CONFIG_ALTERA_PIO is not set
    # CONFIG_DWAPB_GPIO is not set
    # CONFIG_ATMEL_PIO4 is not set
    # CONFIG_LPC32XX_GPIO is not set
    # CONFIG_ROCKCHIP_GPIO is not set
    # CONFIG_VYBRID_GPIO is not set
    
    #
    # I2C support
    #
    # CONFIG_DM_I2C_COMPAT is not set
    # CONFIG_CROS_EC_KEYB is not set
    
    #
    # LED Support
    #
    # CONFIG_LED is not set
    
    #
    # Multifunction device drivers
    #
    # CONFIG_MISC is not set
    # CONFIG_CROS_EC is not set
    # CONFIG_FSL_SEC_MON is not set
    # CONFIG_MXC_OCOTP is not set
    # CONFIG_PWRSEQ is not set
    # CONFIG_PCA9551_LED is not set
    # CONFIG_RESET is not set
    # CONFIG_WINBOND_W83627 is not set
    
    #
    # MMC Host controller Support
    #
    # CONFIG_DM_MMC is not set
    
    #
    # MTD Support
    #
    # CONFIG_MTD is not set
    
    #
    # NAND Device Support
    #
    # CONFIG_NAND_DENALI is not set
    # CONFIG_NAND_VF610_NFC is not set
    # CONFIG_NAND_PXA3XX is not set
    # CONFIG_NAND_ARASAN is not set
    
    #
    # Generic NAND options
    #
    # CONFIG_SPL_NAND_DENALI is not set
    
    #
    # SPI Flash Support
    #
    CONFIG_SPI_FLASH=y
    # CONFIG_SPI_FLASH_BAR is not set
    # CONFIG_SPI_FLASH_ATMEL is not set
    # CONFIG_SPI_FLASH_EON is not set
    # CONFIG_SPI_FLASH_GIGADEVICE is not set
    # CONFIG_SPI_FLASH_MACRONIX is not set
    # CONFIG_SPI_FLASH_SPANSION is not set
    # CONFIG_SPI_FLASH_STMICRO is not set
    # CONFIG_SPI_FLASH_SST is not set
    CONFIG_SPI_FLASH_WINBOND=y
    CONFIG_SPI_FLASH_USE_4K_SECTORS=y
    # CONFIG_SPI_FLASH_MTD is not set
    # CONFIG_DM_ETH is not set
    # CONFIG_PHYLIB is not set
    # CONFIG_NETDEVICES is not set
    
    #
    # PCI
    #
    # CONFIG_DM_PCI is not set
    
    #
    # Pin controllers
    #
    # CONFIG_PINCTRL is not set
    
    #
    # Power
    #
    # CONFIG_DM_PMIC is not set
    # CONFIG_DM_REGULATOR is not set
    # CONFIG_DM_PWM is not set
    # CONFIG_RAM is not set
    
    #
    # Remote Processor drivers
    #
    
    #
    # Real Time Clock
    #
    # CONFIG_DM_RTC is not set
    
    #
    # Serial drivers
    #
    CONFIG_REQUIRE_SERIAL_CONSOLE=y
    CONFIG_SERIAL_PRESENT=y
    CONFIG_SPL_SERIAL_PRESENT=y
    # CONFIG_DEBUG_UART is not set
    # CONFIG_DEBUG_UART_SKIP_INIT is not set
    # CONFIG_ALTERA_JTAG_UART is not set
    # CONFIG_ALTERA_UART is not set
    # CONFIG_FSL_LPUART is not set
    CONFIG_SYS_NS16550=y
    
    #
    # Sound support
    #
    # CONFIG_SOUND is not set
    
    #
    # SPI Support
    #
    # CONFIG_FSL_ESPI is not set
    # CONFIG_TI_QSPI is not set
    # CONFIG_DM_THERMAL is not set
    
    #
    # Timer Support
    #
    # CONFIG_TIMER is not set
    
    #
    # TPM support
    #
    # CONFIG_USB is not set
    
    #
    # Graphics support
    #
    # CONFIG_DM_VIDEO is not set
    
    #
    # TrueType Fonts
    #
    # CONFIG_VIDEO_VESA is not set
    # CONFIG_VIDEO_LCD_ANX9804 is not set
    # CONFIG_VIDEO_LCD_SSD2828 is not set
    # CONFIG_VIDEO_MVEBU is not set
    # CONFIG_DISPLAY is not set
    # CONFIG_VIDEO_BRIDGE is not set
    # CONFIG_PHYS_TO_BUS is not set
    
    #
    # File systems
    #
    
    #
    # Library routines
    #
    # CONFIG_CC_OPTIMIZE_LIBS_FOR_SPEED is not set
    CONFIG_HAVE_PRIVATE_LIBGCC=y
    # CONFIG_USE_PRIVATE_LIBGCC is not set
    CONFIG_SYS_HZ=1000
    # CONFIG_USE_TINY_PRINTF is not set
    CONFIG_REGEX=y
    # CONFIG_LIB_RAND is not set
    # CONFIG_CMD_DHRYSTONE is not set
    # CONFIG_RSA is not set
    # CONFIG_TPM is not set
    
    #
    # Hashing Support
    #
    # CONFIG_SHA1 is not set
    # CONFIG_SHA256 is not set
    # CONFIG_SHA_HW_ACCEL is not set
    
    #
    # Compression Support
    #
    # CONFIG_LZ4 is not set
    # CONFIG_ERRNO_STR is not set
    # CONFIG_UNIT_TEST is not set
    

    Hi,

    we are not using processor SDK we are using Arago krogoth.

    U-boot version: U-Boot 2016.03-00029

    Regards

    Dheeraj

  • Dheeraj,

    This forum supports only official TI's releases like Processor SDK but not Arago. Processor SDK Linux and U-boot 2018.01 can be downloaded at:
    software-dl.ti.com/.../index_FDS.html
    but about "mtest" command please refer to ../u-boot/doc/README.memory-test file description:
    ....................
    There are a number of serious problems with this command:

    - It is terribly slow. Running "mtest" on the whole system RAM
    takes a _long_ time before there is any significance in the fact
    that no errors have been found so far.
    ....................
    Therefore I can conclude that slow execution of "mtest" is expected behavior.

    Regards,
    Tsvetolin Shulev