This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Interfacing OMAP-L138 uPP for 1/2 duplex ADC and DAC operation

Other Parts Discussed in Thread: OMAP-L138, OMAPL138

 

Hello:

I've been poring over the datasheet sprugj5b.pdf  "TMS320C674x/OMAP-L1x Processor Universal Parallel Port (uPP) User's Guide" (see page 12) and

SPRS586B.pdf "OMAP-L138 Low-Power Applications Processor" datasheet (page 243)

 

 

to find a way to configure the uPP to

1) transfer data out to a DAC under DMA control, including 16-bit parallel data and clock OUTPUT, then

2) switching the interface to transfer data in from an ADC under DMA control, including 16-bit parallel data and clock OUTPUT to the ADC.

From the text of the uPP User's Guide (page 12) , it appears that the CLOCK pin for the uPP in receive mode is an input only, while what I require is a clock output to drive the ADC which is synchronous with the START and ENABLE pins presumably provided by the uPP DMA channel.

Is there a way, without external logic, to generate this RECEIVE clock..?

Thanks,

 - Bill