This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NDK and Multicast

I am using the NDK on a networked DM6435 device, which is an Ethernet/IP device.  This protocol uses one-way multicast.  On previous devices, we created a static multicast route in the routing table.  So I believe I need to do the same thing again.

Here is the old VxWorks code:

    /*  Add route to route table, needed for UDP multicast transmission */

    inAddr.s_addr = eips_usersock_getOurIPAddr();

    mRouteAdd("224.0.0.0", inet_ntoa(inAddr), 0, 0, 0);

Here is my attempt with the NDK:
    CI_ROUTE readbackRT;
    // Add the multicast static route
    bzero( &multicastRT, sizeof(multicastRT) );
    multicastRT.IPDestAddr = inet_addr("224.0.0.0");
    multicastRT.IPDestMask = 0;
    multicastRT.IPGateAddr = inet_addr(LocalIPAddr);
    ret = CfgAddEntry( hCfg, CFGTAG_ROUTE, 0, 0, sizeof(CI_ROUTE), (UINT8 *)&multicastRT, 0 );
This doesn't seem to work.
Here is my attempt to read the routing table, this doesn't work either (everything comes back zeros):
        for(int i=0; i <= 2; i++ )
        {
            int tmp = CfgGetImmediate( 0, CFGTAG_ROUTE, 0, i,
                                   sizeof(readbackRT), (UINT8 *)&readbackRT );
        }
Does anybody know how to add a static route and how to read the routing table?  Extra point for knowledge of a correct multicast entry.  Thanks.