This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2G12: DDR_PHY_PGCR1 register in calc tool

Part Number: 66AK2G12

Hello,

WLMODE and PHYHRST bit-fields indicate 1 and 0 respectively in the register calc tool (K2 DDR3 Register Calc v1p60.xlsx), and it looks these have been changed from its default value (WLMODE=0, PHYHRST=1). In the cal tool, those bit-fields are grayed out and the "instruction sheet" suggests it should be the default value.

So my question here is, which values should we use for these bit-fields in DDR3L initialization, the value from the calc tool, or the default value ?

Best Regards,
NK