Part Number: AM6548
Other Parts Discussed in Thread: AM6546,
Tool/software: TI-RTOS
Hello,
I am trying to configure an EP (FPGA) to be able to trigger MSI interrupts on the AM6546 processor (RC). Unfortunately, I am not sure which address should the EP write TLP target.
In the SPRUHY8H for 66AK2G1x processor (Multicore DSP+Arm ® KeyStone II System-on-Chip (SoC)) for example, stands following:
The memory write transactions to generate MSI interrupts in RC are actually targeted at PCIE_MSI_IRQ
register. The MSI interrupt is generated as a result of the one of 32 events that is triggered by a write of
MSI vector value to PCIE_MSI_IRQ register in RC.
The address of the PCIE_MSI_IRQ is available as well (2180 0054h). However, in the SPRUID7B for AM65x/DRA80xM Processors (my RC) there is no mention of such register.
I would appreciate any help.
Best regards,
Dušan