This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3357: MDIO usage for both CPSW and PRU-ICSS

Part Number: AM3357

Hi,

we are running into pinmux pressure and would need to remove the MDIO_PRUSS if at all possible.

A customer is using one RMII interface on the CPSW, and two MII interfaces on PRUSS.

In general can both the RMII connected PHY and the MII connected PHYs be controlled with one MDIO interface, aka the normal MDIO?

Is this still the case when using e.g. a PRU based EMAC_LLD, or would that require teh MDIO_PRUSS?

Is this still the case when e.g. running an Ethercat slave application with Ethercat slave firmware?

Thanks!

--Gunter