Other Parts Discussed in Thread: TMS320C6748
Hi
I am using the TMS320C6748 development kit.
Could you tell me which are the differences between CLKMODE = 0 and CLKMODE 1 because looking at the data sheet
Then there are examples of an On-Chip oscillator
And an internal oscillator
So the point is that taking a look at the dev kit schematic
It seems to be using an exterenal oscillator (Comparing with the previous figures) but if a use CLKMODE = 0, what means On-Chip oscillator instead of CLKMODE = 1 (External oscillator) it Works properly
So i don't know if i am misunderstanding the date sheet, if there is an internal oscillator inside the TMS320C6748 that generate the clock instead of the IC os the last figure or if that IC is working as the On-Chip oscillator.
Could you please explain me the CLKMODEs, which circuit is what and why the DEV KIT Works using On-Chip oscillator?
Thanks in advance,
Juan