Other Parts Discussed in Thread: OMAP3530
Hi,
On my omap3530 project, I've got a camera connected on ISP bus and a USB wifi dongle connected to the USB2 port.
during the ISP acquisition process, both using RGB and YUV pipelines, the USB got this repeated error:
[90261.573638] #
[90261.629791] #
[90261.684204] #
[90261.739166] #
[90261.745941] RTUSB_VendorRequest failed(-110),TxFlags=0x0, ReqType=IN, Req=0x7, Index=0x1104
[90261.793701] #
[90261.848480] #
[90261.903259] #
[90261.957580] #
and the linux OS hangs. If I connect the dongle to the OTG port (musb) the issue doesn't occur.
Any suggestions?
Many thanks.
Andrea