Part Number: AM3354
Tool/software: Linux
Hello,
I am working on AM3354 based custom board which have LCD and touch pannel.
I need to run qt application on it, I have try to run sample demo application of dials and it is running fine.
But for that weston must be running in background, and it shows the Date/Time/Terminal bar on the top of screen.
I need to run that same demo without that top bar, How can I do that?
I have tried to stop weston and try to run dials demo but it is showing below error.
root@am335x-evm:/usr/share/qt5/examples/touch/dials# ./dials
Failed to create display (No such file or directory)
Please do the needful.
Regards,
Ronak