This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Adeos/Xenomai patches for DM36x

I was wondering if anyone had ported the Adeos patches to the Linux kernel included in the DVSDK. The Adeos web site doesn't have patches for the 2.6.32 kernel, and the patches that I've found so far don't apply cleanly. It looks like the OMAP3 is supported, but I haven't seen anything for the DM365.

Thanks,
Frank 

  • Let me try another question. Are there plans to or has anyone ported the Davinci kernel patches to a newer Linux kernel? E.g. 2.6.33 would make it easier for me to pull in the Adeos patches. Or on a slightly different topic, has anyone successfully merged the RT-Preempt patches in with the DVSDK's kernel? I'd like to get a little better real-time performance for part of my application on the DM365, and I'm looking for options to evaluate.