Other Parts Discussed in Thread: OMAP-L138, OMAPL138
Ok so I wasn't particular sure where to put this, but I have a few questions... And before I ask, I'll just say i'm fresh out of college and never really worked on anything like this. But because of a strange oppurnitiy I'm diving head first into this. There is quite a bit I don't know, I just started working with windows ce 6.0 this week, and just learned about the bios/edma3 driver yesterday, and have to figure out how to get it all working.
I'm using an evaluation board, OMAP-L138, with bios 6, I have LLD edma3 1.07.00.01 and 2.00.01.04. I have to get this working on both the ARM in windows CE and the DSP, and I've managed to get the drivers to compile for version 2.00.01.04 but noticed they don't have an example config file for the c6748. Also would I need a different config for the ARM, or is there a config I can use for the OMAP-L138 that will work for both?
If I can't get the config sorted out will the driver 1.07.00.01 work with bios 6?
I feel like I may have to make the config file and if that happens where do I go to start this?
Any help would be greatly appreciated, thanks in advance