Hello,
I'm working around with DM365 evaluation module, and having a problem with encode/decode demo application.
Sorry if I'm asking something very weird since I'm a newbie foreigner.
Result:
Encode demo started.
i2c_adapter i2c-0: TVP2002 - clocks per line detected = 144
Error: Failed to detect video standard, video input connected?
Error: Failed to create video encoder: h264enc
Demo interface started at level 3.
Result of "lsmod":
target $ lsmod
Module                  Size  Used by
dm365mmap               5336  0
edmak                  13192  0
irqk                    8552  0
cmemk                  28172  0
ipv6                  314484  12
Where I am:
I followed "DM365 DVEVM Software Setup" with updated softwares (which are dvsdk_2_10_01_18, psp_02_10_00_14, xdctools 3_15_01_59, and mvl_5_0_0801921_demo). Linux kernel and DVSDK seem to be built fine, and it can be booted via tftp/NFS with bootargs as below.
setenv bootargs console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=$(nfshost):$(rootpath),nolock mem=76M video=davincifb:vid0=OFF:vid1=OFF:osd0=720x576x16,4050K dm365_imp.oper_mode=0 davinci_capture.device_type=4 davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=ntsc
EVM is set to NTSC, and I've connected video component cables to inputs/outputs. Video source is a usual DVD player (and now playing "Life Is a Miracle").
After loading modules with "loadmodules_hd.sh", demo application starts up, and can be displayed and controlled, but fails when I try to start encoding. I've searched for related topics, but could not find the one which fits to my case.
Any hints or suggestions?
Thank you,
Jay