Other Parts Discussed in Thread: DM3730
Hi,
I use the 7 inch LCD panel wiht DM365ZCE30.
I want to know how many size DM365ZCE30 support.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DM3730
Hi,
I use the 7 inch LCD panel wiht DM365ZCE30.
I want to know how many size DM365ZCE30 support.
Thanks
The size of the LCD is not important.
The important factors are the LCD interface and resolution.
The hardware supports any resolution up to pixel rates of about 75MHz in many configurations/resolutions etc...
I have connected a 32" 1366x768 LCD to the DM3xx devices.
If you have a particular LCD in mind then if you can let me know the LCD model number I will check it for you.
It is most likely simply a parallel RGB LCD which can be connected very easily to the DM3xx devices.
BR,
Steve