Part Number: TDA2
Tool/software: TI-RTOS
Hi,
I'm using TDA2x to run the usecase null Src Dec Display and TIDL Object detection using my own input data, every time I run the usecase I got the Decode Error, after reading some other threads from this forum, I noticed that my hdr file contains only zeros which probably cause the Decode Error.(Part of the error is shown below)
[IPU1-0] 29.926554 s: DEC_LINK: outArgs->viddec3OutArgs.extendedError for channel 0 Error: 0x4400
[IPU1-0] 29.926645 s: DEC_LINK: Sequence called number 1
[IPU1-0] 29.959403 s: DECODE: ERROR: ALGPROCESS FAILED (status=0x00004400) !!!
[IPU1-0] 29.959525 s: DEC_LINK: outArgs->viddec3OutArgs.extendedError for channel 0 Error: 0x4400
[IPU1-0] 29.959616 s: DEC_LINK: Sequence called number 2
The OS I'm using is Win7 and I compiled my VSDK using MAKECONFIG=tda2xx_evm_bios_all, I download a sizeBin.exe from other thread but it's not working, so how can I generate my own input data to get the usecase to work?
Thanks~!