Other Parts Discussed in Thread: OMAPL138
Hi everybody,
my setup:
*******Software*********
CCS 4.1.2
C6000 CGT 6.1.16
BIOS 06.21.02.19
EDMA3LLD 02.10.02.03
PSP DRIVER 02.10.00.02
XDC TOOLS 03.16.03.36
IPC 01.00.05.06
XDAIS 06.25.01.08
********Hardware********
LOGIC PD OMAPL138 EVM
At the moment I am trying to merge two RTSC example projects into one. The examples are from
PSP Drivers: video loopback example and EDMA3LLD: edma_drv_bios6_st_sample
Each example works fine for itself on the OMAPL138 EVM. I would like to know what is the best way to merge these two examples together. Each of them uses a config project. Just adding the missing lines in one .cfg file and of course adding the appropriate c files leads to build errors like
"C:/PROGRA~1/TEXASI~1/pspdrivers_02_10_00_02/packages/ti/psp/psc/Psc__prologue.h", line 72: error: identifier "CSL_PscRegsOvly" is undefined The included packages were also updated. So can anyone give some hints how to easy merge two independet examples to one, regarding the dependencies of the examples, so that I get a successful build process. I am thankful for every help and hints. Best regards Gregor