Part Number: TDA2PXEVM
Tool/software: TI-RTOS
Hi,
I'm working on TDA2PX EVM and VisionSDK 3.05 version. I'm giving 4 videos as input using network_rx, then I'm using VPE to convert datafromat to SYSTEM_DF_RGB24_888 and on display side I want Mosaic view of all 4 videos.I referred lvds_vip_multi_cam_view usecase and created a following use-case.
NetworkRx (A15) -> Decode -> VPE -> Dup -> Sync -> Alg_VpeSwMs -> Merge
Dup -> Merge
Merge -> Display_video
GrpxSrc -> Display_Grpx
In AlgorithmLink_VpeSwMsInitQueueInfo API of Alg_VpeSwMsLink_algPlugin.c I added support for RGB format RGB support was not there.
if(pVpeSwMsObj->dataFormat==SYSTEM_DF_RGB24_888
)
{
pVpeSwMsObj->outPitch[0] = maxWidth*3;
pVpeSwMsObj->outPitch[1] = 0;
}
But I get following assertions:
[IPU1-0] 26.971786 s: ** numLvdsCh = 4
[IPU1-0] 26.971847 s:
[IPU1-0] Display type : 9
[IPU1-0] 26.971908 s:
[IPU1-0] DisplayWidth and DisplayHeight : 640 480
[IPU1-0] 26.972000 s: Chains: Using TCP/IP
[IPU1-0] 26.972061 s:
[IPU1-0] **** After SetSyncPrm displayWidth and DisplayHeight : 640 480
[IPU1-0] 26.972152 s: ***Number of channels are 4 ***
[IPU1-0] 26.972213 s:
[IPU1-0] **** After SetAlgVpeSwMsPrm displayWidth and DisplayHeight : 640 480
[IPU1-0] 26.980509 s: IPC_IN_0 : Create in progress !!!
[IPU1-0] 26.981577 s: IPC_IN_0 : Create Done !!!
[IPU1-0] 26.981760 s: DECODE: Create in progress ... !!!
[IPU1-0] 27.020679 s: DECODE: Creating CH0 of 640 x 480 [1] [0],target bitrate = 10000 Kbps ...
[IPU1-0] 27.057189 s: DECODE: Creating CH1 of 640 x 480 [1] [0],target bitrate = 10000 Kbps ...
[IPU1-0] 27.093790 s: DECODE: Creating CH2 of 640 x 480 [1] [0],target bitrate = 10000 Kbps ...
[IPU1-0] 27.130543 s: DECODE: Creating CH3 of 640 x 480 [1] [0],target bitrate = 10000 Kbps ...
[IPU1-0] 27.131367 s: DECODE: All CH Create ... DONE !!!
[IPU1-0] 27.133380 s: DECODE: Create ... DONE !!!
[IPU1-0] 27.133685 s: VPE: Create in progress !!!
[IPU1-0] 27.403861 s: VPE: Loading Down-scaling Co-effs
[IPU1-0] 27.404105 s: VPE: Co-effs Loading ... DONE !!!
[IPU1-0] 27.404349 s: VPE: Create Done !!!
[IPU1-0] 27.405813 s: ALGORITHM: Create in progress (algId = 12) !!!
[IPU1-0] 27.620844 s: CH0: IN:640 x 480 (1920, 1920), OUT:320 x 240 (640, 640)
[IPU1-0] 27.621027 s: CH1: IN:640 x 480 (1920, 1920), OUT:320 x 240 (640, 640)
[IPU1-0] 27.621149 s: CH2: IN:640 x 480 (1920, 1920), OUT:320 x 240 (640, 640)
[IPU1-0] 27.621332 s: CH3: IN:640 x 480 (1920, 1920), OUT:320 x 240 (640, 640)
[IPU1-0] 27.622369 s: vpecore/src/vpscore_vpeCommon.c @ Line 408:
[IPU1-0] 27.622460 s: Data format (20) not supported!!
[IPU1-0] 27.622552 s: vpecore/src/vpscore_vpeApi.c @ Line 453:
[IPU1-0] 27.622613 s: Invalid Parameters!!
[IPU1-0] 27.622704 s: vpedrv/src/vpsdrv_m2mVpeCore.c @ Line 917:
[IPU1-0] 27.622765 s: Set params for VPE core failed!
[IPU1-0] 27.622857 s: vpecore/src/vpscore_vpeApi.c @ Line 642:
[IPU1-0] 27.622948 s: Set the parameter before getting the descriptor info!!
[IPU1-0] 27.623040 s: vpedrv/src/vpsdrv_m2mVpeCore.c @ Line 927:
[IPU1-0] 27.623101 s: Could not get context info for VPE core!
[IPU1-0] 27.623192 s: vpedrv/src/vpsdrv_m2mVpeCore.c @ Line 245:
[IPU1-0] 27.623314 s: Config of core 0 for channel 0 failed.
[IPU1-0] 27.623406 s: vpedrv/src/vpsdrv_m2mVpeApi.c @ Line 908:
[IPU1-0] 27.623467 s: Configuring of cores failed
[IPU1-0] 27.623528 s: Assertion @ Line: 906 in vpeSwMs/vpeSwMsLink_algPlugin.c: retVal == SYSTEM_LINK_STATUS_SOK : failed !!!
[IPU1-0] 27.624046 s: Assertion @ Line: 906 in vpeSwMs/vpeSwMsLink_algPlugin.c: retVal == SYSTEM_LINK_STATUS_SOK : failed !!!
[HOST ] 26.980235 s: NETWORK_RX: NETWORK_RX: Server listening (port=29171) !!!
[HOST ] 26.980387 s: IPC_OUT_0 : Create in progress !!!
[HOST ] 26.980418 s: IPC_OUT_0 : Create Done !!!
How do I add support for RGB format ? How should I proceed with this?
Regards,
Megha .