Tool/software: TI-RTOS
Hello All,
I want to overlay a buffer on display link for which I have created a following usecase,
""""""""""""""""
NetworkRx (A15) -> Alg_Plugin (DSP1) -> Display_Video
OverlayLink (IPU1_0) -> Display_Grpx
""""""""""""""""
OverlayLink is similar to GrpxLink of Vision SDK. But I have used data format type as "SYSTEM_DF_BGR24_888" instead of "SYSTEM_DF_BGR16_565" or "SYSTEM_DF_BGRA16_4444"
In the OverlayLink, I have ported C++ code for overlaying some data. To draw the overlay on display which Vision SDK functions shall I use as the dataformat is SYSTEM_DF_BGR24_888.
I am not able to use "Draw2D_drawPixel" function as there is not support for SYSTEM_DF_BGR24_888 format.
Is there any other function available in Vision SDK which I can use for drawing pixels of SYSTEM_DF_BGR24_888 dataformat.
Regards,
Abhay