Hi ,
The other part is not different from the reference circuit, but the connection of LDQS, LDQS #, UDQS, UDQS # of the second DDR3 (U23) is designed by changing DQS 2 and 3 in the CPU standard.
Is this the part that affects DRAM operation?
If there is a problem, please check if there is a way to resolve by SW change without changing HW.
Please refer to the red part in the figure below.