Part Number: TMS320C6678
Hello,
I`ve run my eyes through the C667x OpenMP runtime and noticed that the runtime enables the prefetch feature for MSMC memory which is configured as cache.
C:\ti\openmp_dsp_c667x_2_06_02_01_debug\packages\ti\runtime\ompbios\OpenMP.c
void __TI_omp_reset_rtsc_mode(void)
{
// Cache configured via ti_sysbios_family_c66_Cache_Module_startup using
// sizes specified in Platform.xdc
//__TI_omp_configure_caches();
/* OMP runtime requires a portion of MSMCSRAM to be non-cached. Since it is
* not possible to disable caching in the MSMCSRAM address range, we need a
* 2 step process:
* 1. Map a portion of MSMCSRAM into a range that can be marked as
* non-cached. This is done using the MPAX register
* 2. Annotate the mapped section as non-cached using the appropriate
* MAR register for that memory range
* All accesses to MSMCSRAM through the mapped address range will not
* be cached.
*/
if (OpenMP_hasMsmc)
{
__TI_setMPAX(OpenMP_mpaxForMsmcMapping,
OpenMP_msmcNoCacheVirtualBase,
OpenMP_msmcNoCachePhysicalBase, 0x10 /* 128 KB */);
__TI_omp_disable_caching(OpenMP_msmcNoCacheVirtualBase,
OpenMP_msmcNoCacheVirtualSize);
/* Enable Caching for MSMCSRAM */
__TI_omp_enable_caching(OpenMP_msmcBase, OpenMP_msmcSize);
}
else
{
__TI_omp_disable_caching(OpenMP_ddrNoCacheBase, OpenMP_ddrNoCacheSize);
}
/* Enable caching for DDR */
__TI_omp_enable_caching(OpenMP_ddrBase, OpenMP_ddrSize);
}
And __TI_omp_enable_caching function in C:\ti\openmp_dsp_c667x_2_06_02_01_debug\packages\ti\runtime\openmp\src\omp_init.c looks like:
void __TI_omp_enable_caching(unsigned int start, unsigned int length)
{
tomp_setMAR(start, length, CACHE_PC|CACHE_PFX|CACHE_WTE);
}
I feel Prefetch should be disabled for MSMC memory because of Errata Advisory 28. It says like this for the workaround:
Software must disable the PFX bits in the MARs for address ranges 0x0C000000 – 0x0FFFFFFF corresponding to cacheable data (MARs can be written to only in supervisor mode. The PFX bit for MARs 12-15 which define attributes for 0x0C000000 – 0x0FFFFFFF is set to 1 by default). This will disable pre-fetching for accesses to those addresses, while still allowing those accesses to be cached in L1D. If pre-fetching for MSMC SRAM and other memory spaces is desired, it can still be done provided they are remapped to a space other than 0x0C00 0000 – 0x0FFF FFFF within the MPAX registers (the remapped MSMC will act as shared level 3 memory and will be cacheable in L1D and L2). The L2 cache must remain on and set to a cache size greater than zero, and must not be frozen when accessing pre-fetchable data, otherwise XMC will apply the previously described L1D-specific behavior for the data prefetcher and subject the system to the same issue.
So, I`ve suggested the customer who is actually using OpenMP runtime to rebuild it with the following customization:
1. Add the following function:
void __TI_omp_enable_caching_withoutPFX(unsigned int start, unsigned int length)
{
tomp_setMAR(start, length, CACHE_PC|CACHE_WTE);
}
2. And replace the existing code with it:
void __TI_omp_reset_rtsc_mode(void)
{
// Cache configured via ti_sysbios_family_c66_Cache_Module_startup using
// sizes specified in Platform.xdc
//__TI_omp_configure_caches();
/* OMP runtime requires a portion of MSMCSRAM to be non-cached. Since it is
* not possible to disable caching in the MSMCSRAM address range, we need a
* 2 step process:
* 1. Map a portion of MSMCSRAM into a range that can be marked as
* non-cached. This is done using the MPAX register
* 2. Annotate the mapped section as non-cached using the appropriate
* MAR register for that memory range
* All accesses to MSMCSRAM through the mapped address range will not
* be cached.
*/
if (OpenMP_hasMsmc)
{
__TI_setMPAX(OpenMP_mpaxForMsmcMapping,
OpenMP_msmcNoCacheVirtualBase,
OpenMP_msmcNoCachePhysicalBase, 0x10 /* 128 KB */);
__TI_omp_disable_caching(OpenMP_msmcNoCacheVirtualBase,
OpenMP_msmcNoCacheVirtualSize);
/* Enable Caching for MSMCSRAM */
// __TI_omp_enable_caching(OpenMP_msmcBase, OpenMP_msmcSize);
__TI_omp_enable_caching_withoutPFX(OpenMP_msmcBase, OpenMP_msmcSize);
}
else
{
__TI_omp_disable_caching(OpenMP_ddrNoCacheBase, OpenMP_ddrNoCacheSize);
}
/* Enable caching for DDR */
__TI_omp_enable_caching(OpenMP_ddrBase, OpenMP_ddrSize);
}
Do you agree with this customization ? If yes, please consider updating the OpenMP runtime in the future release.
Best Regard,
NK